IO-Link: versatile, intelligent, easy to use and... wireless

Reading Time: minutes

Data is now one of the most valuable resources in any enterprise or manufacturing plant. This is because their analysis makes it possible to quickly detect errors, anomalies or defects, and thus reduce downtime and improve production efficiency. How can they be effectively collected, transmitted and analyzed?

The answer is IO-Link, a technology that has revolutionized the world of industrial automation.

What exactly is IO-Link?

IO-Link is a digital communication protocol, which is an ideal example of a solution that meets the challenges of Industry 4.0. It enables the communication of many different automation components. It generates, processes and transmits data, creating a continuous communication system - from the lowest level of the structure of automation systems, e.g. smart sensors or actuators, to control and visualization systems.

Simplifying the definition of the system, we can compare it to a traditional USB link. In this scheme, any USB device works when connected to a USB port, provided that the manufacturers of both devices followed the same rules in the manufacturing process.

How does this technology work?

Speaking in such very general terms, IO-Link is a universal communication protocol through which modern automation devices can generate and transmit a lot of data, not only process data, but also diagnostic data. Modern companies need this data to be able to analyze and interpret it, and then, based on it, to make decisions on optimizing and modifying production processes. These actions serve one specific purpose - business development.

The traditional, i.e. wired, IO-Link solution has some limitations, as small space, mobile applications, complex machine movement or the limitation of the time needed for installation often prevent the location of communication cables. That's why we created its wireless version - IO-Link Wireless.It is one of the first of its kind to take advantage of wireless communication capabilities.

Tomasz Dawid, Marketing Manager

It is worth noting here that IO-Link Wireless does not replace wired solutions, it is only an extension of them, which allows you to enjoy all the advantages of IO-Link solutions - wirelessly.

Why should you lean towards this solution?

IO-Link Wireless, a wireless standard for industrial automation, is a reliable communication method for demanding applications. Unlike other wireless technologies, such as WLAN or Bluetooth, it is designed for industrial needs.

Up to 40 devices can be connected to an IO-Link wireless master with 5 active channels (antennas).This innovative solution, allows users to use a lot of data anytime, anywhere. With very high scalability and adaptability, Balluff's technology is ideal for any plant or machine.

IO-Link Wireless makes it possible to use IO-Link in machine areas where it was not possible before.

Wireless communication

IO-Link Wireless does not replace wired solutions, but is an extension of them that allows you to enjoy all the benefits of IO-Link solutions wirelessly as well.

Keywords

  • IO-Link
  • Sensor technology

Did you like this post?

0

Share this post

Author

Balluff Sp. z o.o.

Balluff Sp. z o.o.

We have been active on the Polish market for more than 25 years. We serve our customers from Pomerania to the Tatra Mountains, providing first-class service and technical support. We are also present online, where we share our knowledge about the latest implementations, industry trends, events or technical aspects of our solutions.


17 Contributions

Comment

More from the author

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.


Balluff Limited

20 Cheshire Business Park
Cheshire Avenue
Lostock Gralam
Northwich, CW9 7UA